SparkFun Electronics Commentsurn:uuid:214d0e4e-f1b1-d287-ce26-ac5b4c9f82492024-03-28T20:14:37-06:00SparkFun ElectronicsToni_K on RTL-09893 - FTDI Basic 3.3V - USB to Serial RetailToni_Kurn:uuid:d75d97c9-a9e0-ce53-ea62-866b375e816c2012-07-05T15:41:56-06:00<p>Sorry for the delayed response. These are pretty reliable little boards, so you shouldn't be seeing any issues with it. If you do run into problems, try reinstalling the drivers first, and if possible, try a different USB cable. If you still have problems, please contact us at techsupport at sparkfun dot com.</p>
Customer #300392 on RTL-09893 - FTDI Basic 3.3V - USB to Serial RetailCustomer #300392urn:uuid:350d37b2-29bd-6350-a239-3f0fd3db02832012-02-09T17:41:04-07:00<p>if some one could prove it worked for them not just me</p>
Customer #300392 on RTL-09893 - FTDI Basic 3.3V - USB to Serial RetailCustomer #300392urn:uuid:b58a2217-7e75-9407-c2df-5103f8186f142012-02-09T17:40:38-07:00<p>The driver link is and has been down for a while found the file though
http://dc168.4shared.com/download/8FuQNqx-/CDM20817_tambolihpagecom.zip?tsid=20120210-003636-927a6953</p>
HolyDiver on RTL-09893 - FTDI Basic 3.3V - USB to Serial RetailHolyDiverurn:uuid:ae95cbf2-0e34-6e81-b08a-0b029720b4d82011-09-06T22:29:48-06:00<p>Questions are never dumb my friend. Not asking a question in fear of ridicule is dumb. However, ridicule is in no way dumb because its a form of hazing and hazing is always fun.</p>
erich81 on RTL-09893 - FTDI Basic 3.3V - USB to Serial Retailerich81urn:uuid:426d78f7-6697-8429-1258-94753bccc4df2011-06-29T09:47:47-06:00<p>dumb question, but are the TX and RX lines on here 3v3 as well?<br>
see dumb question. I see now that yo ucan connect vccio to whatever voltage you want to make it 3.3, 2.8, 5v, etc.</p>
xtalk on RTL-09893 - FTDI Basic 3.3V - USB to Serial Retailxtalkurn:uuid:cda879b2-7e2b-4c6f-5beb-c5a6d852e9342011-04-11T12:20:25-06:00<blockquote>
<p>What's the difference?<br>
This one comes in lovely packaging you can use to impress your friends or wrap as a gift. :)<br>
Otherwise, customer service confirms they are the same board.</p>
</blockquote>
samuel3 on RTL-09893 - FTDI Basic 3.3V - USB to Serial Retailsamuel3urn:uuid:cddc3db1-c5b1-9209-e44b-588ffd10b11f2011-01-19T16:04:07-07:00<p>What's the difference between this one and http://www.sparkfun.com/products/9873 ?<br>
I've afforded the second one and I'm in trouble anytime I try to download an sketch to my Arduino Pro board. I need to press RESET button. Any suggestion?</p>
SomeGuy123 on RTL-09893 - FTDI Basic 3.3V - USB to Serial RetailSomeGuy123urn:uuid:5b0ee8a7-0a6c-c608-698d-b06ab066be342011-01-16T15:36:03-07:00<p>The link on the back of the packaging doesn't lead anywhere.</p>