SparkFun Electronics Commentsurn:uuid:214d0e4e-f1b1-d287-ce26-ac5b4c9f82492024-03-28T04:48:25-06:00SparkFun ElectronicsSTARscream on COM-09933 - 1.0" Single Digit Alphanumeric Display - BlueSTARscreamurn:uuid:5cfcd55e-2dcf-ff43-f333-ffaa26ff6cf62015-06-10T00:15:07-06:00<p>can I get a link to a similar Alphanumerics availble on mouser, digi-key or element14 ?</p>
Akatm7 on COM-09933 - 1.0" Single Digit Alphanumeric Display - BlueAkatm7urn:uuid:2c4f6a70-28c7-396b-92da-dfda567117ee2012-10-23T06:32:10-06:00<p>you don't happen to be related to Adam Savage do you?</p>
Jed Savage on COM-09933 - 1.0" Single Digit Alphanumeric Display - BlueJed Savageurn:uuid:a1338369-a85a-2d00-cbc0-6d3323917fa32012-04-16T18:57:27-06:00<p>Why aren't the decimals connected??</p>
IllogicGate on COM-09933 - 1.0" Single Digit Alphanumeric Display - BlueIllogicGateurn:uuid:9424f11e-f35a-825e-e184-5608416a5eb42011-12-24T15:44:14-07:00<p>Yeah. I HATE it when people put the collector side of an NPN on GROUND. It's controlling stuff COMING INNNNN!!!</p>
thdmtr on COM-09933 - 1.0" Single Digit Alphanumeric Display - Bluethdmtrurn:uuid:759a7b66-acef-d73a-22c0-41e209fc07652011-10-17T10:02:52-06:00<p>oh my god, why anode? it is way easier to control common cathode displays, because we work with positive digital pulses. I gotta ask the same thing about the goddamn useless LATCH hall sensor available here too, so useless, who would need a tiristor-like(latch-state device too) hall effect sensor? I really feel sorry for my money.</p>
lexxmac on COM-09933 - 1.0" Single Digit Alphanumeric Display - Bluelexxmacurn:uuid:2a1ee479-29b1-e50d-99ac-e88e4e9646f42010-09-13T22:45:46-06:00<p>Be Warned: Because these are BLUE and blue LEDs require more voltage and the bigger segments on the display are actually TWO LEDs in series, 5V through the dual-dot segments is <em>barely</em> visible. Meaning, hooking these up to a 5v system (Arduino) isn't quite as easy as you would think.<br>
I'm Going to try this out with a constant current LED driver IC and a little-bitty step-up regulator.</p>
Coyote on COM-09933 - 1.0" Single Digit Alphanumeric Display - BlueCoyoteurn:uuid:6718b73b-e932-61e5-bfa1-ccd6fbd938ae2010-08-16T13:11:29-06:00<p>Heck yeah!<br>
See thread...<br>
<a href="http://forum.sparkfun.com/viewtopic.php?f=5&t=23275" rel="nofollow">http://forum.sparkfun.com/viewtopic.php?f=5&t=23275</a></p>
pressurepoint14@gmail.com on COM-09933 - 1.0" Single Digit Alphanumeric Display - Bluepressurepoint14@gmail.comurn:uuid:9779342f-1012-3339-3237-1d555243f9932010-07-24T11:52:50-06:00<p>if you make a version of this with a serial backpack i will worship the ground you walk on.</p>