The Experiential Robotics Platform (XRP) is a hands-on, comprehensive robotics platform. It includes everything needed to build and program a robot to perform beginner through advanced tasks - building the foundation for innovative thinking, science, engineering, and problem-solving.


Welcome to the World of Experiental Robotics


Add Computer Vision to Your XRP!
Computer vision, simplified—Red Vision adds a touchscreen and camera to the XRP, enabling real-time image processing.
Which XRP Kit Should I Choose?
XRP Kit


Most Comprehensive – No 3D Printing Required
Includes electronics parts plus chassis/plastics for toolless assembly! Also includes a box to store your assembled robot.
You will also need:
DIY Kit


3D Print Your Own Chassis/Plastics
Includes electronics, but not the chassis/plastics to reduce cost - you can 3D print these on your own. Also includes a box to store your assembled robot.
You will also need:
- Computer to code your robot
- Your own 3D Printed Chassis and Plastics
Build-Your-Own Kits


Parts for 30 DIY Kits. Assemble Your Own DIY Kits & 3D Print Chassis/Plastics
Includes electronics for 30 DIY Kits, but not the chassis/plastics - you can 3D print these on your own. Does not include boxes to house the robots.
You will also need:
- Computer to code your robot
- Your own 3D Printed Chassis and Plastics
- Optional: Some sort of box to store your assembled robot
Kit Contents and Parts Glossary
XRP includes:
- 1x XRP Controller
- 1x XRP Chassis Set
- 1x Ultrasonic Distance Sensor
- 1x Custom Line Sensor
- 1x Servo (Sub-Micro Size)
- 2x Hobby Motor with Encoder
- 2x Caster
- 2x O-Ring
- 2x Flexible Qwiic Cable - Female Jumper (4-pin) with Heat Shrink
- 1x Battery Holder - 4xAA to Barrel Jack Connector
- 1x XRP Sticker Sheet


New Features
We've integrated a ton of feedback from the XRP community and made some major upgrades over the beta version.


Streamlined User Experience:
XRP is comprised of four main elements - the hardware kit, online modules, programming environment, and technical forum; the integration of these four components has been streamlined for improved access and overall ease of use.


Enhanced Processing & Memory:
The new XRP Control Board features the RP2350B dual-core processor, providing significantly faster performance and expanded memory (16MB Flash, 8MB PSRAM). This allows for more complex programs and the ability to handle larger datasets, including images.


Expanded Connectivity & Expansion:
Increased GPIO pins (48 total, eight are reserved exclusively for the user), versatile expansion headers compatible with Pico add-on boards, and additional Qwiic connectors significantly enhance electrical connectivity. The RM2 module integrates Wi-Fi and Bluetooth to facilitate wireless control and IoT projects.


Advanced Motor and Servo Control:
New motor drivers with current measurement enable precise torque control, and the number of servo connectors has been doubled to four, allowing more advanced mechanisms.


Improved Controller User Interface:
The control board features a streamlined user interface with a more accessible power switch and button cluster, a modern USB-C connector, a low-voltage indicator, and an RGB LED for user feedback. The design is fully open-source (KiCad).


Optimized and Enhanced Plastics:
The plastic components are optimized for 3D printing, reducing the need for support material and improving durability. The battery holder has been redesigned for secure retention and ease of use. Mounting holes, motor shaft holes, and wire management features add to the platform's versatility. The designs are open-source (Onshape).
Resources & Getting Started
For assembly instructions, online modules, tech support forums and more; xrp.experiential.bot is your basecamp for everything XRP.
Take Your XRP to the Next Level
Once you start with XRP, the possibilities are endless—build more advanced projects, start your own FIRST team, use the XRP for workshops, summer camps, and after-school programs, start your own 3D-printing service — the sky is the limit!
XRP Partners
SparkFun is proud to work with an extraordinary group of partners on the XRP.