Jumper Wires Premium 6" F/F Pack of 10

This is a SparkFun exclusive! These are 155mm long, 26 AWG jumpers with female connectors on both ends. Use these to jumper from any male header on any board, to any other male header. Combine these with our male to male jumpers to create a male to female jumper. Multiple jumpers can be installed next to one another on a 0.1" header. Comes as 1 package of ten jumpers (colors shown).

  • 155mm +/-5mm long
  • 26 AWG

Comments

Looking for answers to technical questions?

We welcome your comments and suggestions below. However, if you are looking for solutions to technical questions please see our Technical Assistance page.

  • SD & khanning: I don't think Sparkfun sells the connectors to build your own cables. They are available at other electronics sites. For example, pololu sells crimping pin for both female and male ends, crimp connector housing for various numbers of pins, and wires with crimp pins attached if you don't want to do the crimping part: http://www.pololu.com/search/compare/19

    Another place to look if you want to make removable cables with 2-10 pins is the wafer pack at dipmicro: http://www.dipmicro.com/store/SET-HDR

  • SD / about 11 years ago / 1

    I will ask the same question khanning asked some time ago. Where can you get the connector parts (both M and F) so one can make custom lengths. The fact that these jumper wires are being made at all suggest the parts exist. I have done a search but can't seem to find any. So where do the folks who make these wires get the parts I wonder?

  • khanning / about 12 years ago / 1

    These are great! Does anyone know where I can just buy some of the female connectors so I can make my own length?

  • ceeeeej / about 13 years ago / 1

    100 pack of F/F 6" jumpers would be ideal for my use.
    What temperature are these rated to? Anyone use these with higher temps, > +85 °C ?

  • pikachu / about 13 years ago / 1

    Really awesome. Will buy again.

  • Member #72840 / about 13 years ago / 1

    What I really need are the wires without the connector bodies and an assortment of single and double row bodies. Then I could build a custom cable between say a bus pirate and JTAG connector without losing the setup each time I need to unplug.

  • nall / about 15 years ago / 1

    I would love to see this product come in other lengths. Possibly a 10" version.

  • Hmmm / about 15 years ago / 1

    So the square part is no larger than 0.1 inches in either direction?
    This is what I need to mate with my mini-grabbers, instead of using bare metal connectors which just fall off.

  • amoore / about 15 years ago / 1

    So what size male contact do these fit--any chance it's a .025-inch square post?

  • schmidtw / about 16 years ago / 1

    I have two packages of these & the M/M adapters - they are a huge time saver & worth every penny.

Customer Reviews

4 out of 5

Based on 1 ratings:

Currently viewing all customer reviews.

Work great

They work great seem to be built well. Not much else to say they are jumpers.