Product Overview
The BBC micro:bit is a credit card sized microcontroller development system, with a very simple and user-friendly visual programming interface, designed to introduce the kids to the world of embedded electronics. The micro:bit project is managed by the micro:bit Educational Foundation. This foundation is a non-profit organization with a very noble goal: giving children around the world a chance to get creative with the technology. You can find more information about the micro:bit project on the official web page.
However, this little development system can be interesting even for more experienced developers, because in its heart, there is a powerful nRF51822 SoC with a 16 MHz ARM Cortex-M0 microcontroller (MCU) with 256 KB Flash and 16 KB RAM, beating. By inserting this ingeniously designed symmetrical development board into the micro:bit Click adapter, the world of possibilities grows exponentially: more than 400 different sensors, displays, drivers, radios, buttons, switches, faders, encoders, relays, converters, and more - neatly packed into the standardized Click board™ form factor, will be just under your fingertips.
Once installed onto the micro:bit Click adapter, the BBC micro:bit can really open the doors to the world of embedded electronics. For those who are more curious, who want to know more: take a peek at the device's datasheet, see which I2C peripheral address is required, which register turns on that BLUE channel of the RGB Driver 3 Click and send in the data. Put the I2C, SPI and Serial communication blocks of the micro:bit IDE to a good use!
Note: BBC's micro:bit is not included in the package.
The micro:bit Click adapter comes comes equipped with two proprietary mikroBUS™ sockets, allowing all the Click board™ devices to be interfaced with the micro:bit with no efforts at all. It is enough to place the small standardized add-on board of your choice on the top of the mikroBUS™ socket - and click it in. That is why this small add-on board is called Click board™ - it just clicks!
The mikroBUS™ standard is founded and maintained by MikroElektronika company, allowing all the various Click boards™ to perfectly fit in, without any compatibility issues. Besides the 3.3V available from the micro:bit itself, the micro:bit Click adapter offers an additional 5V power supply (switchable through the onboard switch), required by some of the Click boards™. This allows interfacing with an extended range of different devices.