Please be aware that this more economical DIY version of the AgXRP Starter Kit does NOT come with a frame. 3D printing files can be found in the Documents section below or you click the link below to purchase an AgXRP Starter Kit that includes a frame. AgXRP Starter Kit - Beta

AgXRP Starter Kit - DIY - Beta
KIT-30713

AgXRP Starter Kit - DIY - Beta

SKU: KIT-30713

Turn your desk into a smart farm with this DIY open-source agricultural robotics kit designed for hands-on STEM education, encouraging customization and 3D printing of your unique frame.

$99.95
In stock
Only 1 left
SKU
KIT-30713
In stock
Stock/Discounts

Please be aware that this more economical DIY version of the AgXRP Starter Kit does NOT come with a frame. 3D printing files can be found in the Documents section below or you click the link below to purchase an AgXRP Starter Kit that includes a frame. AgXRP Starter Kit - Beta

Helpful Documentation

Product Overview

Imagine a classroom where students do not just read about the future of agriculture, they build it. The DIY AgXRP Starter Kit is an open-source, autonomous robotics platform that bridges the gap between STEM education and sustainable farming. By providing the core electronics and encouraging you to 3D-print your own frame, this kit offers an accessible system that turns complex precision agriculture into an engaging, hands-on learning experience. Students will gain practical skills in programming, data analysis, and automation as they design, build, and optimize their own small-scale smart farms.

This kit goes beyond basic robotics by providing an interdisciplinary curriculum that integrates robotics, precision agriculture, and horticultural science, enabling students to tackle real-world farming challenges.

  • Custom Smart Farms: Learn about robotics, agriculture, and 3D printing by constructing your own automated plant care system.
  • Data-Driven Growth: Utilize data analysis, capacitive soil sensors, and peristaltic pumps to optimize crop growth and completely automate watering cycles.
  • Open-Source Access: Gain full access to all 3D printable files, a comprehensive parts list, and detailed assembly instructions to build and modify your system.

As technology in modern farming advances, it’s essential that educational tools evolve to prepare the next generation of farmers to meet global food demands. From coding sensors to optimizing harvest cycles, this kit equips students to explore automation, sustainability, and data-driven agriculture, all while growing their own food and deepening their understanding of the technology shaping our future.

Educator Discount Available: SparkFun and its partners are proud to work closely with the education community. We offer a significant discount on the AgXRP Starter Kit with an Educator account! Please contact support@sparkfun.com to get started.

Hands-On Agricultural Automation

This DIY version of the AgXRP Kit includes the essential electronic hardware and tubing to create a functional, automated plant-care station. However, this economical version does NOT come with a physical frame. You can use our open-source files to 3D-print the enclosures and structural supports yourself!

The SparkFun XRP Controller serves as the brain of your farm, coordinating incoming sensor data and managing the timing of your automation cycles. It features a Raspberry Pi® RP2350B dual-core processor preprogrammed with AgXRP firmware; 16MB of flash and 8MB of PSRAM; a low-power accelerometer + gyroscope 6-DoF IMU (LSM6DSOX from STMicroelectronics®); two Qwiic® connectors for easy integration of sensors and accessories; two dual-channel motor drivers for four motors total; four servo headers; a user button; a full-color RGB LED; 0.1in. headers for electrical expansion possibilities, and more. Wireless connectivity is available via a Raspberry Pi® RM2 radio module, enabling 2.4GHz WiFi and Bluetooth® for remote control and IoT projects.

Instead of just observing a plant, students actively build the systems that keep it healthy.

  • Automated Watering: Students construct a custom peristaltic pump using the Hobby Motor with Encoder, Deep Groove Ball Bearings, and the AgXRP Single Pump Enclosure. This allows for the precise delivery of water through the included Latex Tubing.
  • Accurate Soil Monitoring: The SparkFun Qwiic Soil Moisture Sensor connects to the controller via a Flexible Qwiic Cable to provide real-time data on exactly when a plant needs hydration.
  • DIY Structural Support: You will 3D print the AgXRP frames and enclosures to provide a stable (and potentially custom) foundation for your electronics during long-term experiments.

Looking to expand your setup? You can add up to three AgXRP Pump & Soil Moisture Sensor Expansion Packs to your DIY AgXRP Starter Kit, allowing you to automate and monitor four independent planting zones at the same time.

A fully assembled AgXRP Starter Kit.

Collaborative STEM Ecosystem

To ensure this platform prepares students for real-world challenges, we partnered with organizations driving actual change in communities nationwide. This includes leading academic institutions such as Cornell University and the University of Idaho.

Because this is a Beta release, we are actively looking for educators, students, and community partners to help shape its future. Whether you want to pilot the AgXRP, contribute to curriculum development, or support broader outreach efforts, you are joining a growing community dedicated to building the future of food, one line of code at a time.

The AgXRP partners.

Build Custom Smart Farms with AgXRP.Build Custom Smart Farms with AgXRP.

Custom Smart Farms:

Construct an automated tabletop plant care system that bridges the gap between STEM education and sustainable farming, turning precision agriculture into a hands-on learning experience.

Processing & Memory:

The XRP Controller (with custom AgXRP firmware) features the RP2350B dual-core processor, providing significantly faster performance and expanded memory (16MB Flash, 8MB PSRAM). This allows for more complex programs and the ability to handle larger datasets.

Expanded Connectivity & Expansion provided by the XRP Controller.Expanded Connectivity & Expansion provided by the XRP Controller.

Connectivity & Expansion:

Plenty of GPIO pins (48 total, eight reserved exclusively for the user), expansion headers compatible with Pico add-on boards, and additional Qwiic connectors support up to planting zones. The RM2 module integrates Wi-Fi and Bluetooth to facilitate wireless control and IoT projects.

Data-Driven Automation with AgXRP.Data-Driven Automation with AgXRP.

Data-Driven Automation:

Utilize capacitive soil moisture sensors and construct a custom peristaltic pump to analyze real-time data, optimize crop growth, and completely automate watering cycles.

Improved User Interface with the XRP Controller.Improved User Interface with the XRP Controller.

Controller User Interface:

A control board with a streamlined user interface with an accessible power switch and button cluster, a modern USB-C connector, a low-voltage indicator, and an RGB LED for user feedback. The design is fully open-source (KiCad).

A fully detailed AgXRP Setup & User Guide.A fully detailed AgXRP Setup & User Guide.

Collaborative STEM Ecosystem:

Developed in partnership with organizations like Cornell University and the University of Idaho to provide an interdisciplinary curriculum that prepares students to tackle real-world farming challenges.

Features & Specs

Raspberry Pi RP2350:

  • Dual ARM CortexM33 and Hazard3 RISC-V Processors
  • User-selectable for dual-cores
  • 520kB integrated SRAM in 10 banks
  • 3.3V-tolerant GPIO
  • Peripherals
    • 2x UART
    • 2x SPI
    • 2x I2C
    • 24x PWM Channels
    • 12x PIO State Machines
    • 1 HSTX (High-speed transmit)

Raspberry Pi Radio Module 2:

  • WiFi 4
  • Bluetooth 5.2
  • BDR (1 Mbps)
  • EDR (2 or 3 Mbps)

Qwiic Soil Moisture Sensor:

  • Capacitive sensing over I2C
  • CY8CMBR3102 Controller
    • Software Configurable I2C Address (Default: 0x37)
  • On Board Ruler (Imperial and Metric units)
  • 2x Qwiic Connectors
  • Blue STAT LED (Connects to general-purpose output pin)
  • Red Power LED

XRP Controller:

  • Custom AgXRP Firmware
  • LSM6DSO 6DoF IMU
  • 2x DRV8411A H-Bridge Motor Drivers
  • 4x DC Motor Connectors
  • 4x Servo Motor Connectors
  • 2x Vertical Qwiic Connectors
  • 1x Line Follower Connector
  • 1x Range Sensor Connector
  • 2x 40-pin Expansion Headers
  • 1x 3-pin Debug Header
  • 16MB Flash
  • 8MB PSRAM
  • Power
    • Barrel Jack
    • USB-C
    • Power Switch
  • Buttons
    • RESET
    • BOOT
    • USER
  • LEDs
    • SYS - Red 3.3V Power Status LED
    • MOT - Red 5V Power Status LED
    • LOW VOLT - Red Battery Voltage Indicator LED
    • STAT - Blue LED connected to RM2 IO0
    • RGB - WS2812 RGB LED DataIn connects to RP2350 IO37

Documentation

WARNING: This product may contain chemicals known to the State of California to cause cancer and birth defects or other reproductive harm. See link below for more information. www.P65Warnings.ca.gov

Customer Reviews

All of the parts included in your DIY AgXRP Starter Kit laid out.
AgXRP Starter Kit - DIY - Beta
$99.95
KIT-30713
$99.95 retail price.

Available Discounts

  • $94.95 | 10+ units
  • $89.96 | 25+ units
  • $84.96 | 100+ units

Looking for even larger quantities?

Get in touch for Volume Pricing