Pi Zero USB Stem
KIT-14526

Pi Zero USB Stem

SKU: KIT-14526

The Pi Zero USB Stem is a PCB kit that turns a Raspberry Pi Zero into a USB dongle.

Special Price Current price: $4.95 Regular Price Original price: $9.95
In stock
SKU
KIT-14526
In stock
Stock/Discounts

Product Overview

The Pi Zero USB Stem is a PCB kit that turns a Raspberry Pi Zero into a USB dongle. Once the Stem is installed, your Raspberry Pi can be plugged directly into a computer or USB hub without any additional cables or power supplies. The Raspberry Pi then acts as a USB device using its own Linux kernel gadget drivers to get started.

The Zero Stem is designed to be soldered directly to the USB SMD test pads on the bottom of the Raspberry Pi Zero, needing no wires or pogo pins at all, just solder and a soldering iron! Attaching the stem to your Pi also allows you to create a portable VNC server, or even cluster several Raspberry Pi Zeros with just a USB hub.

The Zero Stem is compatible with the Raspberry Pi Zero v1.3 and the Raspberry Pi Zero W v1.1, but unfortunately it is not compatible with the Raspberry Pi Zero v1.2 or any full-size Raspberry Pi due to their shapes and sizes.

Note: In order for your Pi Zero to function as a USB device with this Stem, you will need to configure it to act as one. You will be able to find these instructions in the Documentations tab under "How to OTG Fast".

Features & Specs

Documentation

WARNING: This product may contain chemicals known to the State of California to cause cancer and birth defects or other reproductive harm. See link below for more information. www.P65Warnings.ca.gov

Customer Reviews

Pi Zero USB Stem
Pi Zero USB Stem
Special Price Current price: $4.95 Regular Price Original price: $9.95
KIT-14526
$4.95 retail price.

Looking for even larger quantities?

Get in touch for Volume Pricing