Raspberry Pi Zero W
DEV-14277

Raspberry Pi Zero W

SKU: DEV-14277

The Raspberry Pi Zero W is still the Pi you know and love, but at a largely reduced size of only 65mm long by 30mm wide and still at a low price!

$16.50
Out of stock
SKU
DEV-14277
Out of stock
Stock/Discounts

Helpful Documentation

Product Overview

The credit-card-sized computer has become even smaller! The Raspberry Pi Zero W is still the Pi you know and love, but at a largely reduced size of only 65mm long by 30mm wide and at a very economical price. With the addition of wireless LAN and Bluetooth, the Raspberry Pi Zero W is ideal for making embedded Internet of Things (IoT) projects. The Pi Zero W has been designed to be as flexible and compact as possible with mini connectors and an unpopulated 40-pin GPIO, allowing you to use only what your project requires.

At the heart of the Raspberry Pi Zero W is a 1GHz BCM2835 single-core processor with 512MB RAM. Quite frankly, this Pi is about four times faster that the original Raspberry Pi and is only a fraction of the cost of the current RPi3.

The setup for the Raspberry Pi Zero W is a little more complicated than on other Pis. Because of the small size, many of the connectors on the Pi Zero are not standard. For starters you will want a Mini HDMI to HDMI cable or adapter to connect to your monitor. You will also need a USB OTG cable to connect a USB device, as well as a unique CSI camera cable. No matter how you want to use your Raspberry Pi Zero W, you will need a microSD card with an operating system and a high-quality 5V power supply to power your board.

Important: The Raspberry Pi Zero W is limited to one unit per customer account.

Features & Specs

  • 802.11 b/g/n wireless LAN
  • Bluetooth(R) 4.1
  • Bluetooth Low Energy (BLE)
  • 1GHz, single-core CPU
  • 512MB RAM
  • Mini HDMI and USB On-The-Go ports
  • Micro USB power
  • HAT-compatible 40-pin header pins
  • Composite video and reset headers
  • CSI camera connector

Documentation

WARNING: This product may contain chemicals known to the State of California to cause cancer and birth defects or other reproductive harm. See link below for more information. www.P65Warnings.ca.gov

Customer Reviews

Raspberry Pi Zero W
Raspberry Pi Zero W
$16.50
DEV-14277
$16.5 retail price.

Looking for even larger quantities?

Get in touch for Volume Pricing