XRP Beta End-of-Life Sale: This product is part of the discontinued SparkFun XRP Beta line and is on a final closeout sale while supplies last. Stock is limited.

Important: This EoL status applies only to Beta versions. The full production XRP line remains available. All orders for this item placed after November 11, 2025, will be considered non-cancelable and non-returnable. Product Discontinuation Notice

This product has been retired from our catalog and is no longer for sale. View the updated version below. KIT-28011

Notice: This is the Beta version of the XRP DIY Kit. While this is still a great assortment of essential robotics hardware, the latest version can be found below: Experiential Robotics Platform (XRP) - DIY Kit
Experiential Robotics Platform (XRP) - DIY Kit - Beta
KIT-24045

Experiential Robotics Platform (XRP) - DIY Kit - Beta

SKU: KIT-24045

The XRP Robotics Platform is a hands-on, comprehensive robotics platform and includes everything needed to build and program a beginner to advanced robot.

Out of stock
SKU
KIT-24045

XRP Beta End-of-Life Sale: This product is part of the discontinued SparkFun XRP Beta line and is on a final closeout sale while supplies last. Stock is limited.

Important: This EoL status applies only to Beta versions. The full production XRP line remains available. All orders for this item placed after November 11, 2025, will be considered non-cancelable and non-returnable. Product Discontinuation Notice

This product has been retired from our catalog and is no longer for sale. View the updated version below. KIT-28011

Notice: This is the Beta version of the XRP DIY Kit. While this is still a great assortment of essential robotics hardware, the latest version can be found below: Experiential Robotics Platform (XRP) - DIY Kit

Helpful Documentation

Product Overview

The Experiential Robotics Platform (XRP) is a hands-on, comprehensive robotics platform and includes everything needed to build and program a robot to perform beginning through advanced tasks - building the foundation for innovative thinking, science, engineering, and problem solving. The platform provides:

  • Progression from fundamental robotics to driving, line following, using sensors, using a robotic arm, and culminates in building an autonomous delivery robot
  • Coding environment includes Blockly tools/libraries, Python, and the FIRST ® Robotics coding development tool, WPILib
  • Easy-to-assemble hardware kit that can be assembled completely tool free (no soldering, no screws)
  • Online activities and modules that build on one another
  • Content designed for middle and high-school students and beginners
  • Jumping off point for customizing the robot in countless ways
Educator and FIRST Team Discount Available: SparkFun and its partners are proud to work closely with the education community. We offer a significant discount on the XRP Robotics Platform Kit with an Educator account, including FIRST teams. Please contact support@sparkfun.com to get started.

This kit is the hardware arm of the XRP. At the heart of it is the XRP Controller Board, which includes an on-board Raspberry Pi® Pico W featuring the RP2040 microcontroller; low-power accelerometer + gyroscope 6-DoF IMU (LSM6DSOX from STMicroelectronics®); a Qwiic® connector for easy integration of sensors and accessories; two dual-channel motor drivers for four motors total; two servo headers; a momentary button switch; and more. The kit also includes an ultrasonic rangefinder, line follower, two motors with encoders, servo motor, Qwiic cables, two casters, two o-rings, and a battery holder. The robot is normally powered by 4xAA batteries (not included in the kit), but any supply up to 11V is supported via the barrel connector.

This more economical DIY version of the XRP Kit does NOT come with a chassis. Encouraging you to print and use your own.

The online modules, accessible at experientialrobotics.org, were developed by Worcester Polytechnic Institute (WPI) through its OpenSTEM platform and serve as a comprehensive introduction to robotics. The modules and content progression have been tested with hundreds of users and have been refined to the current form, which is still in beta. The content offers a fun, engaging experience and asks users to solve real-world robotics challenges.

This kit and the online tools are in beta form – by using the kits now, you will not only be an early adopter, but you will be able to provide feedback to make the platform better.

Contributing Partners for XRP

Features & Specs

Kit Includes:

  • 1x XRP Controller Board
  • 1x Ultrasonic Distance Sensor
  • 1x Servo (Sub-Micro Size)
  • 2x Hobby Motor with Encoder
  • 2x Caster
  • 2x O-Ring
  • 2x Flexible Qwiic Cable - Female Jumper (4-pin) with Heat Shrink
  • 1x Battery Holder - 4xAA to Barrel Jack Connector
  • 1x Custom Line Follower Board
  • 1x XRP Sticker Sheet

Documentation

WARNING: This product may contain chemicals known to the State of California to cause cancer and birth defects or other reproductive harm. See link below for more information. www.P65Warnings.ca.gov

Customer Reviews

Experiential Robotics Platform (XRP) - DIY Kit - Beta
Experiential Robotics Platform (XRP) - DIY Kit - Beta KIT-24045
$45 retail price.

Looking for even larger quantities?

Get in touch for Volume Pricing