XRP Beta End-of-Life Sale: This product is part of the discontinued SparkFun XRP Beta line and is on a final closeout sale while supplies last. Stock is limited.

Important: This EoL status applies only to Beta versions. The full production XRP line remains available. All orders for this item placed after November 11, 2025, will be considered non-cancelable and non-returnable. Product Discontinuation Notice

Notice: This is the Beta version of the XRP Controller. While this is still a great robotics controller, the latest version can be found below: SparkFun Experiential Robotics Platform (XRP) Controller
SparkFun Experiential Robotics Platform (XRP) Controller - Beta
ROB-22727

SparkFun Experiential Robotics Platform (XRP) Controller - Beta

SKU: ROB-22727

At the heart of the Experiential Robotics Platform (XRP) lies the powerful yet easy-to-use XRP Controller Board, the brains of the XRP.

Special Price Current price: $25.00 Regular Price Original price: $49.95
In stock
SKU
ROB-22727
In stock
Stock/Discounts

XRP Beta End-of-Life Sale: This product is part of the discontinued SparkFun XRP Beta line and is on a final closeout sale while supplies last. Stock is limited.

Important: This EoL status applies only to Beta versions. The full production XRP line remains available. All orders for this item placed after November 11, 2025, will be considered non-cancelable and non-returnable. Product Discontinuation Notice

Notice: This is the Beta version of the XRP Controller. While this is still a great robotics controller, the latest version can be found below: SparkFun Experiential Robotics Platform (XRP) Controller

Helpful Documentation

Product Overview

The Experiential Robotics Platform (XRP) is a hands-on, comprehensive robotics platform and includes everything needed to build and program a robot to perform beginning through advanced tasks - building the foundation for innovative thinking, science, engineering, and problem solving. The platform provides:

  • Progression from fundamental robotics to driving, line following, using sensors, using a robotic arm, and culminates in building an autonomous delivery robot
  • Coding environment includes Blockly tools/libraries, Python, and the FIRST ® Robotics coding development tool, WPILib
  • Easy-to-assemble hardware kit that can be assembled completely tool free (no soldering, no screws)
  • Online activities and modules that build on one another
  • Content designed for middle and high-school students and beginners
  • Jumping off point for customizing the robot in countless ways
Educator and FIRST Team Discount Available: SparkFun and its partners are proud to work closely with the education community. We offer a significant discount on the XRP Robotics Platform Kit with an Educator account, including FIRST teams. Please contact support@sparkfun.com to get started.

At the heart of the Experiential Robotics Platform (XRP) lies the powerful yet easy-to-use XRP Controller Board. This board is the brains of the XRP, packed with features that empower you to bring your robotic creations to life.

Connect your robot to the world wirelessly with the built-in Raspberry Pi Pico W, enabling seamless WiFi and Bluetooth® connectivity for remote control and data exchange. Navigate complex maneuvers with precision thanks to the onboard 6-axis motion sensor, which tracks your robot's every move and orientation. Control up to four motors independently with the integrated dual-channel drivers, perfect for powering wheels, tracks, or even robotic arms. You can even attach up to two servo motors to add a gripper or manipulator for precise and controlled movements.

There are endless customization possibilities with the Qwiic connector. This simple interface makes adding sensors and accessories a breeze, allowing you to tailor your robot's capabilities to your needs.

The XRP Controller Board caters to all skill levels. Choose from beginner-friendly Blockly or dive deeper with Python. Even FIRST® Robotics enthusiasts can utilize familiar tools to program their creations. With multiple programming options available, the possibilities are truly endless.

So, whether you're a seasoned robotics expert or just starting your journey, the XRP Controller Board empowers you to build, program, and control robots that can explore, interact, and even learn. Its powerful features, ease of use, and expandability make it the perfect platform to learn, teach, and unleash creativity.

This board and the online tools are in beta form – by using the Controller now, you will not only be an early adopter, but you will be able to provide feedback to make the platform better.

Contributing Partners for XRP

Features & Specs

Raspberry Pi Pico W:

  • RP2040 microcontroller chip designed by Raspberry Pi in the United Kingdom
  • Dual-core ARM Cortex M0+ processor, flexible clock running up to 133 MHz
  • 264kB of SRAM, and 2MB of on-board Flash memory
  • Infineon CYW43439 Based Wireless Module
  • USB 1.1 Host and Device support
  • Low-power sleep and dormant modes
  • Accurate clock and timer on-chip
  • Temperature sensor
  • Accelerated floating point libraries on-chip

XRP Controller:

  • LSM6DSO 6DoF IMU
  • DRV8835 H-Bridge Motor Driver
  • 4x DC Motor Connectors
  • 2x Servo Motor Connectors
  • 1x Vertical Qwiic Connector
  • 1x Line Follower Connector
  • 1x Range Sensor Connector
  • 1x Extra Connector
  • PWR & GND Pins
  • GPIO28 & GPIO22 Pins for Pico W
  • Power
  • Barrel Jack
  • microB USB (On Pico W)
  • Power Switch

Documentation

  • XRP Robotics Platform Home Page (Online Modules

    WARNING: This product may contain chemicals known to the State of California to cause cancer and birth defects or other reproductive harm. See link below for more information. www.P65Warnings.ca.gov

Customer Reviews

SparkFun Experiential Robotics Platform (XRP) Controller - Beta
SparkFun Experiential Robotics Platform (XRP) Controller - Beta
Special Price Current price: $25.00 Regular Price Original price: $49.95
ROB-22727
$25 retail price.

Looking for even larger quantities?

Get in touch for Volume Pricing