Accelerometer, Gyro and IMU Buying Guide
Movement sensors are everywhere now, utilize one in your project today!
Accelerometers
What's an accelerometer measure? Well, acceleration. You know...how fast something is speeding up or slowing down. You'll see acceleration displayed either in units of meters per second squared (m/s2), or G-force (g), which is about 9.8m/s2 (the exact value depends on your elevation and the mass of the planet you're on).
Accelerometers are used to sense both static (e.g. gravity) and dynamic (e.g. sudden starts/stops) acceleration. One of the more widely used applications for accelerometers is tilt-sensing. Because they are affected by the acceleration of gravity, an accelerometer can tell you how it's oriented with respect to the Earth's surface. For example, Apple's iPhone has an accelerometer, which lets it know whether it's being held in portrait or landscape mode. An accelerometer can also be used to sense motion. For instance, an accelerometer in Nintendo's WiiMote can be used to sense emulated forehands and backhands of a tennis racket, or rolls of a bowling ball. Finally, an accelerometer can also be used to sense if a device is in a state of free fall. This feature is implemented in several hard drives: if a drop is sensed, the hard drive is quickly switched off to protect against data loss.
Now that you know what they do, let's consider what characteristics you should be looking for when selecting your accelerometer:
Accelerometer Range
The upper and lower limits of what the accelerometer can measure is also known as its range. In most cases, a smaller full-scale range means a more sensitive output; so you can get a more precise reading out of an accelerometer with a low full-scale range.
You want to select a sensing range that will best fit your project, if your project will only be subjected to accelerations between +2g and -2g, a ±250g-ranged accelerometer won't give you much, if any, precision.
We have a good assortment of accelerometers, with maximum ranges stretching from ±1g to ±250g. Most of our accelerometers are set to a hard maximum/minimum range, however some of the fancier accelerometers feature selectable ranges.
Accelerometer Interface
This is another one of the more important specifications. Accelerometers will have either an analog, pulse-width modulated (PWM), or digital interface.
- Accelerometers with an analog output will produce a voltage that is directly proportional to the sensed acceleration. At 0g, the analog output will usually reside at about the middle of the supplied voltage (e.g. 1.65V for a 3.3V sensor). Generally this interface is the easiest to work with, as analog-to-digital converters (ADCs) are implemented in most microcontrollers.
- Accelerometers with a PWM interface will produce a square wave with a fixed frequency, but the duty cycle of the pulse will vary with the sensed acceleration. These are pretty rare; we've only got one in our catalog.
- Digital accelerometers usually feature a serial interface be it SPI or I²C. Depending on your experience, these may be the most difficult to get integrated with your microcontroller. That said, digital accelerometers are popular because they usually have more features, and are less susceptible to noise than their analog counterparts.
Number of axes measured in accelerometers
This one's very straightforward: out of the three axes possible (x, y, and z), how many can the accelerometer sense? Three-axis accelerometers are usually the way to go; they are the most common and they are really no more expensive than equivalently sensitive one or two axis accelerometers.
Accelerometer Power Usage
If your project is battery powered, you might want to consider how much power the accelerometer will consume. The required current consumption will usually be in the 100s of µA range. Some sensors also feature sleep functionality to conserve energy when the accelerometer isn't needed.
Accelerometer Bonus Features
Many more recently developed accelerometers may have a few nifty features, beyond just producing acceleration data. These newer accelerometers may include features like selectable measurement ranges, sleep control, 0-g detection, and tap sensing.
Gyroscopes
Gyroscopes measure angular velocity, how fast something is spinning about an axis. If you're trying to monitor the orientation of an object in motion, an accelerometer may not give you enough information to know exactly how it's oriented. Unlike accelerometers gyros are not affected by gravity, so they make a great complement to each other. You'll usually see angular velocity represented in units of rotations per minute (RPM), or degrees per second (°/s). The three axes of rotation are either referenced as x, y, and z, or roll, pitch, and yaw.
In the past, gyros have been used for space navigation, missile control, under-water guidance, and flight guidance. Now they are starting to be used alongside accelerometers for applications like motion-capture and vehicle navigation.
A lot of what was considered when selecting an accelerometer still applies to selecting the perfect gyro:
Gyroscope Range
Make sure the maximum angular velocity you're expecting to measure doesn't exceed the maximum range of the gyro. But also, in order to get the best possible sensitivity, make sure your gyro's range isn't much greater than what you're expecting.
Gyroscope Interface
There's actually not much diversity in this section, 95% of the gyros we have feature an *analog *output. There are a few that have a digital interface - either SPI or I2C.
Number of Axes Measured in Gyroscope
Compared to accelerometers, gyros are a little behind the curve. Only recently have inexpensive, 3-axis gyros begun to appear on the market. Most of our gyros are either 1- or 2-axis. When selecting those, you need to pay attention to which of the three axes the gyro will measure; for example, some two axis gyros will measure pitch and roll, while others measure pitch and yaw.
Gyroscope Power Usage
If your project is battery powered, you might want to consider how much power the gyro will consume. The required current consumption will usually be in the 100s of µA range. Some sensors also feature sleep functionality to conserve energy when the gyro isn't needed.
Gyroscope Bonus Features
Not much in this section is going to blow you away. Many gyros feature a temperature output, which is very useful when compensating for drift.
IMUs (Inertial Measurement Unit)
Gyroscopes and accelerometers are great, but alone they don't give you quite enough information to be able to comfortably calculate things like orientation, position, and velocity. To measure those and other variables many people combine the two sensors, to create an inertial measurement unit (IMU) which provides two to six degrees of freedom (DOF). IMUs are widely used in devices that require knowledge of their exact position, for example robotic arms, guided missiles, and tools used in the study of body motion.
SparkFun's IMUs can really be broken down into two classes: simple IMU combo boards, which just mount an accelerometer and gyro onto a single PCB, and more complex units that interface a microcontroller with the sensors to produce a serial output. If you've glanced over the previous sections, you should know what kind of specifications to be looking for in IMUs: the number of axes (both for the accelerometer and gyro), the measuring range of the sensors, and the interface.
Accelerometers, Gyros, and IMUs
Resources section
Optional short lead-in to the section just to tell them what kind of resources we have in store for them.


Description of what the resource is. Please make sure to link both the image and title and put ALT text on the image as well!


Description of what the resource is. Please make sure to link both the image and title and put ALT text on the image as well!


Description of what the resource is. Please make sure to link both the image and title and put ALT text on the image as well!