Track My Order
Frequently Asked Questions
International Shipping Info
Send Email
added to your cart!
The SparkFun NEO-M9N GPS Breakout is a high quality GPS board with equally impressive configuration options through Dead Reck…
The BBC micro:bit v2 is a pocket-sized computer that has been updated with additional features that let you get creative with…
The LilyPad ProtoSnap Plus is a sewable electronics prototyping board that you can use to explore circuits and programming, t…
The SparkFun Servo Trigger is a small robotics board that simplifies the control of hobby RC servo motors. When an external s…
This polarized I2C cable insulation is made from silicon making it more flexible than our original Qwiic cable particularly i…
The digital multimeter (DMM) is an essential tool in every electronic enthusiasts arsenal. The SparkFun Digital Multimeter, h…
The SparkFun OpenLog with Headers can store, or "log", huge amounts of serial data and act as a black box of sorts.
This hot-air rework station is great for professionals and hobbyists in need of tight temperature tolerances and large air fl…
The XRP Robotics Platform is a hands-on, comprehensive robotics platform and includes everything needed to build and program …
The 915MHz SiK Telemetry Radio V3 is a lightweight and inexpensive open source radio platform that can allow for ranges of 30…
This is a 10 pack of Biomedical Sensor Pads, disposable electrodes that can be used to measure EEG, ECG and EMG levels. these…
The SparkFun VR IMU Breakout is a cutting-edge triple-axis accelerometer/gyro/magnetometer in a single package that you can c…
This is your tried and true white solderless breadboard. It has 2 power buses, 10 columns, and 30 rows - a total of 400 tie i…
This great GT-521F52 fingerprint module from ADH-Tech communicates over TTL Serial so you can easily embed it into your next …
This straight bar load cell (sometimes called a strain gauge) can translate up to 10kg of pressure (force) into an electrical…
The Raspberry Pi 4 Desktop Kit (8GB) includes everything you need to turn any monitor with an HDMI port into a desktop PC.
If you’re ready to step your Arduino game up from older 8-bit/16MHz microcontrollers, the SparkFun SAMD21 Mini Breakout is …
If you are not needing a lot of power to start your FPGA adventure, or are looking for a more economical option, the Alchitry…
This is a time saving kit of 140 jumper wires - cut, stripped, and pre-bent for your prototyping pleasure.
These are very slim, extremely light weight batteries based on Lithium Ion chemistry. Each cell outputs a nominal 3.7V at 850…
This is the E-textile Basics Lab Pack, a basic wearables learning kit that can easily get you and a group of peers or student…
The PINECIL Soldering Iron Kit provides a compact powerhouse and everything you need to ignite your DIY dream.
The TMC6300 from Trinamic is a powerful, yet easy to use three-phase brushless DC (BLDC) motor driver.
Arduino is an open-source physical computing platform based on a simple i/o board and a development environment that implemen…
Here is a simple, low-cost, high quality servo for all your mechatronic needs. This servo is very similar in size and specifi…
The SparkFun Pro Micro RP2040 is a low-cost, high performance board with flexible digital interfaces featuring the Raspberry …
The 8GB Raspberry Pi 4 features the ability to run two 4k resolution monitors, to run true Gigabit Ethernet operations, all a…
This 10K trimmable potentiometer has a small knob built right in and it's breadboard friendly to boot!
The EasyDriver is a simple to use stepper motor driver, compatible with anything that can output a digital 0 to 5V or 0 to 3.…
The SparkFun MicroMod GNSS carrier board has the accuracy of GNSS Real Time Kinematics (RTK) with the flexibility of the Micr…
This economical sensor provides 2cm to 4m of non-contact measurement functionality with a ranging accuracy that can reach up …
This is the FemtoBuck, a small-size single-output constant current LED driver. Each FemtoBuck has the capability to dim a sin…
The SparkFun Buck-Boost Converter is a handy power accessory board that allows you to fine tune the amount of power your proj…
These are 6" long jumper wires with male connectors on both ends. Use these to jumper from any female header on any board, to…
This is the latest version of our popular through-hole Simon Says Kit. We've made some changes to the board that should make …
This is the newest revision of our [FTDI Basic](https://www.sparkfun.com/products/retired/8772). We now use a SMD 6-pin heade…
This is a breakout board for the very handy 16-Channel Analog/Digital Multiplexer/Demultiplexer CD74HC4067. This chip is like…
The SparkFun Beginner Parts Kit is a small container of frequently used parts that gives you all of the basic components you…
The new Raspberry Pi 27W USB-C PD (Power Delivery) Power Supply will deliver a maximum of 5.1V, 5A enabling the RPi 5 to powe…
This disc load cell (sometimes called a strain gauge) can translate up to a whopping 200kg of pressure (force) into an electr…
The SparkFun 9DoF IMU Breakout combines a high-performance 6DoF IMU with the highly sensitive triple-axis magnetometer in a Q…
The SparkFun Qwiic ToF Imager is built around VL53L5CX from ST Electronics; a state of the art, Time-of-Flight (ToF), multizo…
The SparkFun Pro nRF52840 Mini is a development board for Nordic’s nRF52840 – a powerful combination of ARM Cortex-M4 CPU…
The SparkFun Qwiic SerLCD is a serial enabled LCD that provides a simple and cost effective solution for adding a 16x2 RGB on…
This is a kit that provides you with a basic assortment of capacitors to start or continue your electronics tinkering. No mo…
The Teensy 4.1 with Headers features an ARM Cortex-M7 processor at 600MHz, 4x larger flash memory than the 4.0, and optional …
These are a pair of hobby gearmotors from DAGU. These gearmotors are the same ones recommended for use in the Shadow Chassis …
The SparkFun OpenLog Artemis is an open source data logger that comes pre-programmed to automatically log sensor, GPS, serial…