This product has been retired from our catalog and is no longer for sale. We recommend the SparkFun RTK Facet as a comparable product. GPS-19984

Important! u-blox is discontinuing the PointPerfect L-Band service for North America on December 31, 2025. The RTK Facet L-Band remains compatible with standard correction services that connect via the internet.

SparkFun RTK Facet L-Band
GPS-20000

SparkFun RTK Facet L-Band

SKU: GPS-20000

The Facet L-Band is a surveying receiver that can receive RTK corrections directly from satellites, with no Internet connection or Base Station required.

Out of stock
SKU
GPS-20000

This product has been retired from our catalog and is no longer for sale. We recommend the SparkFun RTK Facet as a comparable product. GPS-19984

Important! u-blox is discontinuing the PointPerfect L-Band service for North America on December 31, 2025. The RTK Facet L-Band remains compatible with standard correction services that connect via the internet.

Helpful Documentation

Product Overview

Notice: This product has been retired due to the upcoming sunset of the PointPerfect L-Band service, which will end on December 31, 2025. Active L-Band subscriptions will remain functional until that date. This device can still receive corrections via IP-based services such as PointPerfect Flex or other compatible IP correction sources.

Designed and manufactured in Boulder, Colorado, USA, the SparkFun RTK Facet L-Band is your one-stop shop for high precision geolocation and surveying needs. For basic users, it’s incredibly easy to get up and running; for advanced users, the RTK Facet L-Band is a flexible and powerful tool. With just the press of a button, the RTK Facet L-Band is the fastest way to take centimeter-grade measurements. With built-in corrections, 14mm Real Time Kinematic fixes are less than a minute away. By connecting your phone to the RTK Facet L-Band over Bluetooth®, your phone or tablet can receive the NMEA output and work with most GIS software. This is exactly how $10,000 surveying devices have been operating for the past decade - we just made it faster, more precise, and a lot more economical.

The RTK Facet L-Band works with common GIS software for Android and iOS including SW Maps (Android / iOS), ArcGIS Survey123, Field Genius, SurvPC, Survey Master, Vespucci, QGIS, QField (Android / iOS), and any GIS software that supports NMEA over Bluetooth or TCP.

The RTK Facet L-Band utilizes corrections from u-blox's PointPerfect service broadcast from a geosynchronous Inmarsat satellite. The only setup required is a WiFi SSID and password. Once entered, the device will provision itself and periodically (once a month) update the decryption keys necessary to use the PointPerfect service. The price of the RTK Facet L-Band includes a 12-month subscription. Additional years of service can be purchased.

Under the hood of the SparkFun RTK Facet L-Band is an ESP32 WROOM connected to a ZED-F9P GNSS receiver, a NEO-D9S L-Band receiver (for corrections), and a variety of peripheral hardware (LiPo fuel gauge, microSD, etc). Additionally, housed under the dome of the RTK Facet L-Band is a surveyor grade L1/L2/L-Band antenna. This antenna is a unique combination of elements designed to receive the GNSS signals (L1/L2) alongside the 1.55GHz PointPerfect corrections. The built-in antenna has an ARP of 69mm from the base to the measuring point of the L1 antenna and an ARP of 68mm to the measuring point of the L2 antenna. The RTK Facet L-Band is programmed in Arduino and can be tailored by you to fit whatever your needs may be.

This device can be used in five modes:

  • GNSS Positioning (~30cm accuracy) - also known as 'Rover'
  • GNSS Positioning with RTK L-Band (1.4 to 6cm accuracy) - also known as 'Rover with L-Band RTK Fix'
  • GNSS Positioning with RTK (1.4cm accuracy) - also known as 'Rover with RTK Fix'
  • GNSS Base Station
  • GNSS Base Station NTRIP Server

At Power On the device will enter Rover or Base mode; whichever state the device was in at the last power down. When the POWER/SETUP button is pressed momentarily, a menu is presented to change the RTK Facet L-Band to Rover or Base mode. The display will indicate the change with a small car or flag icon.

In Rover mode the RTK Facet L-Band will check if WiFi is available and update any L-Band keys needed (keys expire every 56 days). The device will automatically begin receiving and decrypting position correction data. Simultaneously, the RTK L-Band will receive L1 and L2 GNSS signals from the four constellations (GPS, GLONASS, Galileo, and BeiDou). The device will calculate the position based on the combination of GNSS and correction signals. The receiver will quickly (within 60 seconds) obtain an RTK float, then fix. Similar to a standard grade GPS receiver, the RTK Facet L-Band will output industry standard NMEA sentences at 4Hz and broadcast them over any paired Bluetooth® device. The end user will need to parse the NMEA sentences using commonly available mobile apps, GIS products, or embedded devices (there are many open source libraries). Unlike standard grade GPS receivers that have 2500mm accuracy, the accuracy in this mode is approximately 14 to 60mm horizontal positional accuracy.

If the device is in Rover mode but L-Band is not available, regular RTCM based RTK is still available. When RTCM correction data is sent over Bluetooth® or into the radio port, the device will automatically enter Positioning with RTK mode. In this mode RTK Facet L-Band will receive L1/L2 signals from the antenna and correction data from a base station. The receiver will quickly (within a second) obtain an RTK float, then fix. The NMEA sentences will have increased accuracy of 14mm horizontal and 10mm vertical accuracy. The RTCM correction data is most easily obtained over the Internet using a free app on your phone (see SW Maps or Lefebure NTRIP) and sent over Bluetooth® to the RTK Facet L-Band but RTCM can also be delivered over an external cellular or radio link to a 2nd RTK Facet, Surveyor, Express, etc setup as a base station.

In Rover mode the RTK Facet L-Band will receive L1 and L2 GNSS signals from the four constellations (GPS, GLONASS, Galileo, and BeiDou) and calculate the position based on these signals. Similar to a standard grade GPS receiver, the RTK Facet L-Band will output industry standard NMEA sentences at 4Hz and broadcast them over any paired Bluetooth® device. The end user will need to parse the NMEA sentences using commonly available mobile apps, GIS products, or embedded devices (there are many open source libraries). Unlike standard grade GPS receivers that have 2500mm accuracy, the accuracy in this mode is approximately 300mm horizontal positional accuracy.

In Base mode the device will enter Base Station mode. This is used when the device is mounted to a fixed position (like a tripod or roof). The RTK Facet L-Band will initiate a survey. After 60 to 120 seconds the survey will complete and the RTK Facet L-Band will begin transmitting RTCM correction data out the radio port. A base is often used in conjunction with a second RTK Facet L-Band (or RTK Surveyor, Express, Express Plus, etc) unit set to 'Rover' to obtain the 14mm accuracy. Said differently, the Base sits still and sends correction data to the Rover so that the Rover can output a really accurate position.

In addition to supplying position data the RTK Facet L-Band is capable of logging NMEA, RAWX, and SFRBX for post processing making it ideal for research and advanced positioning applications.

The RTK Facet L-Band is an open source hardware product meaning you can fully obtain, see, and even modify the electrical and mechanical design files. This allows for easier maintenance and repair over time.

The SparkFun RTK Facet L-Band kit includes everything you need: the enclosed device, correction subscription for 6 months, thread adapter, charger, data cables, and carrying case. It does NOT include a surveying pole. These items will need to be purchased separately.

Important: The PointPerfect L-Band subscription compatible with this product will not be operational past December 31, 2025.
The SparkFun RTK Facet L-Band is not designed for permanent outdoor mounting. Please use the RTK mosaic-X5 or the RTK Reference Station that is located inside or protected from the elements. Or, for a DIY solution, the ESP32 attached to our ZED-F9P breakout is a great way to go. See our How to Build a DIY GNSS Reference Station tutorial for more information.

Includes:

Features & Specs

MODULE RECEPTION CONSTELLATIONS INTERNAL ANTENNA BATTERY RUNTIME COMMUNICATIONS HARDWARE APPLICATION CORRECTIONS SOURCE
u-blox ZED-F9P L1/L2 GPS, GLONASS, Galileo, BeiDou Yes [int battery] Bluetooth, Radio Base or Rover PointPerfect L-Band, NTRIP

Overall Device Specs:


  • Enclosed Facet Design IP53 - Protected from limited dust ingress and water spray
  • Internal Antenna: L1/L2/L-Band with ≥5dBi gain
  • Internal Battery: LiPo 6Ah with fast 1 amp charging
  • Radio Port: 3.3V TTL Serial (57600bps RTCM TX/RX)
  • Data Port: 3.3V TTL Serial (115200bps NMEA)
  • Qwiic Port: Supports I2C based add-on devices
  • microSD: Compatible up to 32GB
  • Embedded OLED Display for positional accuracy, available satellites, data logging, etc.
  • Single push button control
  • Weight: 598g (1.3 lbs)
  • Dimensions: 136mm x 146mm x 80mm (5.35in x 5.74in x 3.14in)
  • Works with common GIS software including: SW Maps, SurvPC, Field Genius, et al.
  • Open Source Hardware Certified Project
  • Manufactured in Boulder, CO USA

GNSS Receiver Specs:



GNSS Receiver: ZED-F9P

  • Concurrent reception of GPS, GLONASS, Galileo, and BeiDou
  •  Receives both L1C/A and L2C bands
  •  184-channel u-blox F9 engine
  •  Current: 68mA - 130mA (varies with constellations and tracking state)
  •  Time to First Fix: 25s (cold), 2s (hot)
  •  Max Navigation Rate:
    •  PVT (basic location over UBX binary protocol) - 25Hz
    •  RTK - 20Hz
    •  Raw - 25Hz
  •  Horizontal Position Accuracy:
    •  2.5m without RTK 
    • 0.010m with RTK
  •  Max Altitude: 50km (31 miles)
  • Max Velocity: 500m/s (1118mph)

Satellite Data Receiver: NEO-D9S

  • L-Band data receiver compliance: SESTB28A
  • Frequency range: 1525 to 1559MHz
  •  Sensitivity: 133dBm
  •  Current: 35 - 130mA (varies during acquisition and tracking state)
  •  Time to First Frame: <10s
  •  Receives PMP messages from Inmarsat Geosynchronous Satellites

 

Supported GIS Data Collector Software:

 

Documentation

Antenna Phase Center:

  • L1: 68.0mm
  • L2: 69.0mm
  • Average: 68.5mm

Schematics:

Additional Resources:

WARNING: This product may contain chemicals known to the State of California to cause cancer and birth defects or other reproductive harm. See link below for more information. www.P65Warnings.ca.gov

Customer Reviews

SparkFun RTK Facet L-Band
SparkFun RTK Facet L-Band GPS-20000
$1099.95 retail price.

Available Discounts

  • $1,044.95 | 10+ units
  • $989.96 | 25+ units

Looking for even larger quantities?

Get in touch for Volume Pricing