XRP LogoXRP Logo

The Experiential Robotics Platform (XRP) is a hands-on, comprehensive robotics platform. It includes everything needed to build and program a robot to perform beginner through advanced tasks - building the foundation for innovative thinking, science, engineering, and problem-solving.

Experiential Robotics PlatformExperiential Robotics Platform

Add Computer Vision to Your XRP!

Computer vision, simplified—Red Vision adds a touchscreen and camera to the XRP, enabling real-time image processing.

XRP with Red Vision BoardXRP with Red Vision Board

Assembled XRP with Red Vision Kit

Which XRP Kit Should I Choose?


 XRP Kit  

Full XRP KitFull XRP Kit

Most Comprehensive – No 3D Printing Required

Includes electronics parts plus chassis/plastics for toolless assembly! Also includes a box to store your assembled robot. 


You will also need: 

- 4x AA Batteries

- USB-C cable

- Computer to code your robot 

DIY Kit  

XRP DIY KitXRP DIY Kit

3D Print Your Own Chassis/Plastics 

Includes electronics, but not the chassis/plastics to reduce cost - you can 3D print these on your own. Also includes a box to store your assembled robot. 


You will also need: 

- 4x AA Batteries

- USB-C cable

- Computer to code your robot

- Your own 3D Printed Chassis and Plastics 

Build-Your-Own Kits  

XRP Set of 30XRP Set of 30

Parts for 30 DIY Kits. Assemble Your Own DIY Kits & 3D Print Chassis/Plastics 

Includes electronics for 30 DIY Kits, but not the chassis/plastics - you can 3D print these on your own. Does not include boxes to house the robots.  


You will also need: 

- 4x AA Batteries

- USB-C cable

- Computer to code your robot

- Your own 3D Printed Chassis and Plastics 

- Optional: Some sort of box to store your assembled robot

New Features


We've integrated a ton of feedback from the XRP community and made some major upgrades over the beta version.

XRP User ExperienceXRP User Experience

Streamlined User Experience:

XRP is comprised of four main elements - the hardware kit, online modules, programming environment, and technical forum; the integration of these four components has been streamlined for improved access and overall ease of use.

RP2350 on XRPRP2350 on XRP

Enhanced Processing & Memory:

The new XRP Control Board features the RP2350B dual-core processor, providing significantly faster performance and expanded memory (16MB Flash, 8MB PSRAM). This allows for more complex programs and the ability to handle larger datasets, including images.

XRP GPIOXRP GPIO

Expanded Connectivity & Expansion:

Increased GPIO pins (48 total, eight are reserved exclusively for the user), versatile expansion headers compatible with Pico add-on boards, and additional Qwiic connectors significantly enhance electrical connectivity. The RM2 module integrates Wi-Fi and Bluetooth to facilitate wireless control and IoT projects.

XRP servo slotsXRP servo slots

Advanced Motor and Servo Control:

New motor drivers with current measurement enable precise torque control, and the number of servo connectors has been doubled to four, allowing more advanced mechanisms.

XRP controller boardXRP controller board

Improved Controller User Interface:

The control board features a streamlined user interface with a more accessible power switch and button cluster, a modern USB-C connector, a low-voltage indicator, and an RGB LED for user feedback. The design is fully open-source (KiCad).

XRP snap on connectorsXRP snap on connectors

Optimized and Enhanced Plastics:

The plastic components are optimized for 3D printing, reducing the need for support material and improving durability. The battery holder has been redesigned for secure retention and ease of use. Mounting holes, motor shaft holes, and wire management features add to the platform's versatility. The designs are open-source (Onshape).

Resources & Getting Started


For assembly instructions, online modules, tech support forums and more; xrp.experiential.bot is your basecamp for everything  XRP.

XRP Controller OverviewXRP Controller Overview

View the Complete Hardware Overview for the (XRP) Controller.

Code the XRPCode the XRP

Whether you are just getting started with Blockly or you are experienced with MicroPython, XRP has resources for you to improve your coding skills.

XRP 3D Print DesignsXRP 3D Print Designs

See how the XRP community has expanded its capabilites with unique and creative 3D models.

Take Your XRP to the Next Level


Once you start with XRP, the possibilities are endless—build more advanced projects, start your own FIRST team, use the XRP for workshops, summer camps, and after-school programs, start your own 3D-printing service — the sky is the limit!

XRP Controller OverviewXRP Controller Overview

XRP for Summer Camps, Workshops and After-School Programs

XRP Controller OverviewXRP Controller Overview

XRP for the FIRSTⓇ Community: Camps, Outreach, Recruitment, and Off-Season Skill Building

XRP Controller OverviewXRP Controller Overview

Use AgXRP for Agriculture Education - Build a Soil Moisture System

XRP 3D Print DesignsXRP 3D Print Designs

XRP for Summer Camps, Workshops and After-School Programs

XRP Partners


SparkFun is proud to work with an extraordinary group of partners on the XRP.

XRP PartnersXRP Partners